This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1794A: 48KHz, 24bit的I2S数据格式下无输出

Part Number: PCM1794A
Other Parts Discussed in Thread: NE5534

您好,我在尝试使用PCM1794A和TAP3130D制作功放。上电测试后差分电流没有输出,我已经尝试了第二版设计了,这个问题让我很疑惑。

I2S数据由SOC提供,示波器测试显示,MCK为12.2878MHz,BCK为3.072MHz,LRCK为47.99KHz。PCM1794A的MONO、DEM、CHSEL、FTM0、FMT1均由10K电阻拉低至地。MUTE信号也拉低至地。

I/V Stage的运放使用LM4562MA,万用表测试显示只有5.7mA的直流电流,设计参考了基于INA1620和OPA1612的Hi-Fi耳机放大器方案

问题可能是由于什么导致的?

希望能得到解答,感谢!