Part Number: TPA3110D2-Q1
每个通道可以支持多大的峰值电流,负载4 ohm,电压12V的情况下
TRANSLATE with x
English
TRANSLATE with
Enable collaborative features and customize widget: Bing Webmaster Portal
Back
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3110D2-Q1
每个通道可以支持多大的峰值电流,负载4 ohm,电压12V的情况下
在12Vdc和4欧姆负载下,您需要3%的Apeak电流和1%的THD。这些设备不会限制这种电流。