Other Parts Discussed in Thread: LMK61E2
你好,我们购买了LMK61E2EVM开发板,用USB供电,频谱仪与clk_out_p连接测试开发板的输出时钟,然后频谱仪MARK到中心频点156.25MHz后将频宽设置为200Hz,VBW设置为3Hz,发现也会有几十到上百Hz的漂移,如附件,请问正常么,谢谢;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们购买了LMK61E2EVM开发板,用USB供电,频谱仪与clk_out_p连接测试开发板的输出时钟,然后频谱仪MARK到中心频点156.25MHz后将频宽设置为200Hz,VBW设置为3Hz,发现也会有几十到上百Hz的漂移,如附件,请问正常么,谢谢;
您好
只是确认一下,频谱分析仪的跨度是否设置为200Hz?对于156.25MHz的时钟信号,50Hz的偏差对应于约0.32ppm的误差,这似乎是LMK61E2的合理漂移水平。
您提到只有OUTP连接到频谱分析仪,为了获得最佳性能,时钟信号的P端和N端都应该终止。如果你有平衡-不平衡转换器,我建议在进入频谱分析仪之前使用它将差分时钟信号转换为单端。如果你没有平衡-不平衡转换器,你也可以尝试在OUTN上添加一个50欧姆的GND端子。如果信号的P端和N端没有正确端接,可能会出现过度反射/其他信号完整性问题,从而干扰频谱测量。
您好
很抱歉这里的回复延迟了,我们的工作台设置上周被其他测量占用了。我在LMK61E2EVM上测试了这一点,我看到了与视频类似的行为,频率在几分钟内漂移了高达50Hz左右。正如我在第一次回复中提到的,50Hz对应约0.32ppm的误差,因此这在该设备的正常漂移范围内。如果你还有其他问题,请告诉我。