LMX2594: Signal spurious emissions

Part Number: LMX2594


The required frequency range for our point-frequency signal is 10 MHz to 1.2 GHz, with a harmonic suppression requirement of greater than 50 dBc for the output signal. Therefore, we connected a low-pass filter (model: LFCG-1200+) to the output port RFoutA. We observed that when the output port matching is poor and the OUTx_PWR is set to any value between 28 and 31, the spectrum shows not only the fundamental signal but also subharmonic signals at half and one-and-a-half times the fundamental frequency, with very high output power. However, when OUTx_PWR is set between 1 and 27, these subharmonic signals disappear. This phenomenon occurs specifically in the frequency range of 1.13 GHz to 1.19 GHz and is not observed in other frequency bands.

We would like to ask:

  1. Why does this phenomenon occur?

  2. Why is it only observed in the 1.13 GHz to 1.19 GHz range and not in other frequency bands?

The observed phenomenon is as follows:

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    这可能是由于低通滤波器引起的信号反射,因此它可能与输出功率和频率有关。我不建议在合成器之后立即进行滤波。如果我们在合成器之后进行滤波,我建议在合成器和滤波器之间添加一个10dB的衬垫。该焊盘为反射信号提供了额外的隔离/衰减,最大限度地减少了对VCO的影响。

  • 感谢您的回复。

    我们的不匹配是在滤波器输出端接可拆卸SMA接头引起的,去该滤波器官网找了相关的数据手册,该滤波器从DC-1200MHz匹配都挺好的,麻烦你们再看一下,帮我们分析一下。此外二分之一次的基波和二分之三次的基波产生的原因,麻烦你们帮我们也分析一下,谢谢。

    合成器输出后接的低通滤波器与SMA头:

  • 您好

    分频后的输出是方波,因此信号中包含了很多谐波。当然,基波信号会通过滤波器。然而,其他谐波要么被分流到地,要么被反射。

    如果您的原理图与我们的评估板相似,您可以尝试为C6使用不同的值,或者在C6并联添加几个不同值的电容器。

    L1,尝试使用电感器或铁氧体磁珠或0Ω电阻器。

  • 好的,谢谢您的回答,我们的原理图与开发板是类似的,对于您提供方法我们去尝试一下。

    另外,在测试过程中(还是在不匹配的情况下)我们发现通过控制输出频点的输出功率可以消除该现象(即调整pow的值),输出功率为最大及附近时(pow为某个范围)就存在该现象,输出功率较小时就不存在该现象。麻烦帮我们分析一下。

    对于二分之一次的基波和二分之三次的基波产生的原因还存在疑惑。

  • 您好

    我认为这很有道理,更高的输出功率设置会带来更多的反射功率,从而导致干扰更加严重。

    还有一件事你可以尝试。将OUT_ISET从默认值0调整为3。这将使输出功率降低约2dB。

  • 好的,谢谢,我们尝试一下。您提供的方法是帮助我们消除该现象,能不能帮我们分析一下该现象产生的原因呢?

  • 您好

    这很可能会导致信号被反射到压控振荡器(VCO)上,从而中断设备的运行。

  • 好的,谢谢您的回答