This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: LMX2594输出存在375M\1125M杂散

Part Number: LMX2594

你好:

我在使用LMX2594时,参考频率选择为100MHz,使能OSCin 倍频器,Fpd=200MHz,选择VCO4=12GHz,仅使能OUTPUT A,分频器配置为4,输出3GHz,框图如下;

频谱仪测试3GHz输出,发现375MHz杂散和1125M杂散,通过寄存器R0,设置成0x2519,power downLMX2594时杂散消失;

Lmx2594的配置如下:

地址  值

0x00 251A 复位寄存器,10ms后取消复位
0x00 2518
0x4E 0003
0x4D 0

0x4C 000C
0x4B 0840
0x4A 0
0x49 003F
0x48 1
0x47 0081
0x46 C350
0x45 0
0x44 03E8
0x43 0
0x42 01F4
0x41 0
0x40 1388
0x3F 0
0x3E 0322
0x3D 00A8
0x3C 0
0x3B 1
0x3A 9001

0x39 0020
0x38 0
0x37 0
0x36 0
0x35 0
0x34 0820
0x33 0080
0x32 0
0x31 4180
0x30 0300
0x2F 0300
0x2E 07FC
0x2D C0DF

0x2C 1F80
0x2B 0
0x2A 0
0x29 0
0x28 0
0x27 1
0x26 0
0x25 0104
0x24 003C
0x23 4
0x22 0
0x21 1E21
0x20 0393
0x1F 43EC
0x1E 318C
0x1D 318C
0x1C 0488
0x1B 2
0x1A 0DB0
0x19 0C2B

0x18 071A
0x17 007C
0x16 1
0x15 0401
0x14 E848
0x13 27B7
0x12 0064
0x11 012C
0x10 0080
0xF 064F
0xE 1E70
0xD 4000
0xC 5001
0xB 0018
0xA 10D8
0x9 1604
0x8 2000

0x7 40B2
0x6 C802
0x5 00C8
0x4 0A43
0x3 0642
0x2 0500
0x1 0808