This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: 实现多个LMK04828输出的时钟同步

Part Number: LMK04828

我需要做一块时钟验证板卡,它有7颗LMK04828,我的主控制板要放一颗,两块底板A,B上各放一颗,每块底板上各插两个FMC子卡,FMC子卡上也放一个LMK04828,我就是希望每个FMC子板上的LMK04828最终输出的ADC采样时钟和SYSREF是相位对齐的 。目前我的控制方案是,主控板C上是这样的,从CLKIN1输入一个外部的低频信号,从OSCIN输入VCXO(CVHD-950-122P880)产生的时钟,然后控制板C产生两对设备时钟(DCLKOUT)和SYSREF(SDCLKOUT)分配给板卡A和板卡B。设备时钟从板卡A和板卡B的上的LMK04828的CLKIN1输入,SYSREF从CLKIN0输入。这个时候A和B上的LMK04828需要再分别产生两对设备时钟(DCLKOUT)和SYSREF(SDCLKOUT),分配给A上的两块FMC子卡,两块子卡上分别插着有一个LMK04828,B也同理。最终四块FMC子卡上的LMK04828输出的采样时钟和SYSREF需要保证同步 。

您可以评估一下我的原理图是否有问题吗?我想知道这7颗LMK04828都需要VCXO吗 

clock_validation_board.pdf