Part Number: LMX2594
我的应用是LMX2594的A路输出10MHz及以上频率,B路的输出后面接一个分频器产生10MHz以下的频率,扫频的时候经常出现的一个问题是跨10MHz时A路没有输出信号,比如扫频范围是1MHz~11MHz,总共扫9个点。此时测量LD信号也是高电平,但测量射频信号却没有输出。我是用的全辅助模式。我尝试把AB两路用同一条指令进行开、关切换没有解决问题,尝试把AB两路同时保持开启也没有解决问题。请问可能是什么原因?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2594
我的应用是LMX2594的A路输出10MHz及以上频率,B路的输出后面接一个分频器产生10MHz以下的频率,扫频的时候经常出现的一个问题是跨10MHz时A路没有输出信号,比如扫频范围是1MHz~11MHz,总共扫9个点。此时测量LD信号也是高电平,但测量射频信号却没有输出。我是用的全辅助模式。我尝试把AB两路用同一条指令进行开、关切换没有解决问题,尝试把AB两路同时保持开启也没有解决问题。请问可能是什么原因?谢谢!