This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: LMK04832如何实现跨板时钟同频同相

Part Number: LMK04832

您好:

我们在使用LMK04832设计一个多片AD同步采集系统时,遇到了相位差不固定问题,现在有两个问题想确认一下:

1、在输入时钟同源相参时钟的情况下,多片LMK04832的输出时钟在上下电初始化过程中,是否会存在相位偏差,且偏移量是输入时钟的整数倍。例如:两片04832输入400MHz的时钟,输出10MHz时钟的边沿之间会存在相位偏移,偏移量是**输入时钟周期的整数倍**(400MHz 周期 = 2.5ns),相位差范围 0~100ns(10MHz 周期)之间随机。 

2、如果要做到多片LMK04832同时使用时,输出的时钟相位差固定,是否需要将所有芯片的SYNC管脚连接到一起,并输入一个统一的触发信号?请推荐多片LMK04832同时使用时,输出时钟相位偏差固定的硬件设计方案(原理图或框图)。

祝好!