CDCLVC1106: 芯片无输出

Part Number: CDCLVC1106
Other Parts Discussed in Thread: ADS131M04

芯片供电3.3V,1G引脚串联10K电阻接入3.3V电源,输入采用有源晶振,频率8.192MHz,芯片输出给ADC芯片ADS131M04。测试发现1106芯片6路均没有输出,电平为0V。

1、测量输入正常,方波,幅度3.3V。

2、供电和1G控制正常。

3、输出线路没有低阻短路等情况,阻抗正常。

4、设计中芯片3个电源引脚,只有一个引脚加了0.1uF和1uF电容,其他两个电源引脚直接由PCB电源层接入3.3V,不知道是不是这个问题导致。请帮助分析,谢谢!