Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCE6214
Hello, I would like to consult about the use of CDCE6214. At present, I cannot realize the control of CDCE6214 chip. In detail: In order to bypass the reading and writing of eeprom, only the register set of the chip is written. At the same time, HW_SW_CTRL and REFSEL have been connected to the MCU on the hardware circuit, so the IO pins connected to the MCU are configured to high resistance state to realize the dangling state of HW_SW_CTRL and REFSEL. Let the chip enter the backoff mode. The voltage of the two pins measured by the multimeter is 1.6V, so it is confirmed that the state is M and the backoff mode has been entered. Then I used IIC to write the CDCE6214RGER register, but after a lot of tests, only a few registers were written correctly, and the values of the other registers were not the values I set. For example, the operation of first pulling PDN and then reading and writing register R43 can realize the reading and writing of the register, which shows the timing correctness of IIC, but when writing other registers, most of them have errors. In addition, the register group values (R0-R85) are obtained by TICSPRO software. Therefore, I would like to ask if there is anything else I have not considered. I hope to get a reply,thank you.