Part Number: TPL5010
1.如果TPL5010发出了俩个WAKE信号,MCU这边没有回复DONE,TPL5010是否就会使能rstn
2.比如时序: ...TWAKE1...TDONE1.....TWAKE2....TWAKE3...
那么TPL5010是否在TWAKE3+20ms才会使能RSTN,还是在TWAKE2就会使能RSTN
3.TPL5010上电后,MCU这边如果一直没发DONE信号,会不会有问题
4.TPL5010 RSTN上如果只有50KΩ的上拉,会不会有问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPL5010
1.如果TPL5010发出了俩个WAKE信号,MCU这边没有回复DONE,TPL5010是否就会使能rstn
2.比如时序: ...TWAKE1...TDONE1.....TWAKE2....TWAKE3...
那么TPL5010是否在TWAKE3+20ms才会使能RSTN,还是在TWAKE2就会使能RSTN
3.TPL5010上电后,MCU这边如果一直没发DONE信号,会不会有问题
4.TPL5010 RSTN上如果只有50KΩ的上拉,会不会有问题
您好,
1.是的。
2. 如果MCU没有回复DONE信号的话,不会有下一个WAKE信号的。因为收不到DONE信号,TPL5010 会使能RST信号。
20ms的意思是在下一个WAKE到来之前至少20ms,MCU回复DONE信号。
3,一直没有发DONE信号,那么MCU处于复位状态。If the DONE signal is not asserted, the TPL5010 asserts the RSTn signal to reset the µC.
4.最好通过GPIO控制RSTN的时序。