Other Parts Discussed in Thread: CDCE913,
这款芯片能不能做一路98.304M时钟输出,以及一路由VCO控制的24.576M的时钟输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,因为不知您的输入频率是多少,我这边是 TI Clock Pro 软件默认的输入频率27MHz,输出98.304M或者以及一路输出24.576Mhz的配置如下。您可以参考一下。另外,TIClock Pro的下载链接:https://www.ti.com.cn/cn/lit/zip/scac073

您好,我这边默认输入频率也是27MHz,我这边项目需求是需要两路时钟输出,一路固定的98.304MHz,另外一路是压控输出98.304MHz,这样的需求这款芯片可以满足吗
您好,您的意思是一路VCO直接输出吗?但是通过上述配置您可以看出,当输出为98.304MHz的时候,VCO频率为196.6Mhz。通过配置分频系数Pdiv输出98.3Mhz,直接输出98.3MHz是不行的,另外,只需要一路输出的话,可以考虑CDCE913,3路输出,它和CDCE937的差别在于937含有3个PLL, 7路输出。
您好,关于+-150ppm的pulling range,参考晶振是27Mhz,请参考这篇关于CDCE9xx系列的VCXO Application Guideline 应用手册,其中P4给出了关于pulling range的具体介绍:https://www.ti.com/lit/an/scaa085a/scaa085a.pdf