This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: LMX2572 Full Assist 模式低温下失锁问题

Part Number: LMX2572


LMX2572 在室温下VCO Calibration了150个频点,回读了VCO_SEL_FORCE,VCO_CAPCTRL_FORCE,VCO_DACISET_FORCE 值保存在MCU的flash中,在-40度低温下给LMX2572上电依次设置150个频点,发现有约1/3的LMX2572的部分频点失锁,问题可能出在哪里?

  • 您好,

    您的意思是有约1/3的LMX2572异常吗?您测试了多少个设备

    还是说有约1/3的频点(50个频点)失锁?

  • 8个设备,每个设备上有2个lmx2572,其中两个设备上的两个lmx2572都有部分频点失锁,有两个设备上只有一个lmx2572部分频点失锁,每个lmx2572在零下40度冷启动失锁的频点数量不一样,有2个lmx2572只发现了一个频点失锁,有3个lmx2572发现了不到10个频点失锁,有1个lmx2572发现10个以上频点失锁。另外我怀疑有更多失锁频点没有被发现,-40度测试150个频点,失锁的频点都在前50个频点内,我怀疑测试到后面的频点时设备本身的发热已经使lmx2572正常锁定了。我还在-30度进行了测试,全部lmx2572都正常。

  • 您好,为更加有效地解决您的问题,我询问了更了解这款芯片的TI资深工程师,他还没有给反馈,一旦得到回复会立即回复给您

  • 您好,已给反馈,他说您的怀疑是合理的,电路中引脚 3 , 27 和 38 处的去耦电容是多少