Part Number: LMX2594
Other Parts Discussed in Thread: REG101
器件1和器件2参考信号来自同一个时钟,SYNC连接到了一起,通过程序控制给器件1和2写入一样的程序,外部通过脉冲信号控制SYNC,输出没有锁定,当加脉冲后,频率输出也没相参。将寄存器Reg 58 中的15位配置为0,当外部SYNC产生脉冲后,电电流会增加,但还是没有锁住。配置就是按这个官方配置的,环路也是一样的。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
void SendReg1(void)
{
SendOneReg1(0x70,0x00,0x00); //0111 0000 1111 1111 1111 1111 //Reg112
SendOneReg1(0x6F,0x00,0x00);
SendOneReg1(0x6E,0x00,0x00);
SendOneReg1(0x6D,0x00,0x00);
SendOneReg1(0x6C,0x00,0x00);
SendOneReg1(0x6B,0x00,0x00);
SendOneReg1(0x6A,0x00,0x01); //0110 1010 0000 0000 0000 0001 //Reg106 RAMP_SCALE_COUNT=1
SendOneReg1(0x69,0x00,0x21); //0110 1001 0000 0000 0010 0001 //Reg105 RAMP_DLY_CNT=1 RAMP1_NEXT_TRIG=1
SendOneReg1(0x68,0x00,0x00);
SendOneReg1(0x67,0x00,0x00);
SendOneReg1(0x66,0x00,0x00);
SendOneReg1(0x65,0x00,0x11); //0110 0101 0000 0000 0001 0001 //Reg101 RAMP1_RST=1 RAMP0_NEXT_TRIG=1
SendOneReg1(0x64,0x00,0x00);
SendOneReg1(0x63,0x00,0x00);
SendOneReg1(0x62,0x00,0x00);
SendOneReg1(0x61,0x08,0x88); //0110 0001 0000 1000 1000 1000 //Reg97 RAMP0_RST[15]=0 RAMP_TRIGB[10:7]=0001 RAMP_TRIGA[6:3]=0001 RAMP_BURST_TRIG[1:0]=00
SendOneReg1(0x60,0x00,0x00);
SendOneReg1(0x5F,0x00,0x00);
SendOneReg1(0x5E,0x00,0x00);
SendOneReg1(0x5D,0x00,0x00);
SendOneReg1(0x5C,0x00,0x00);
SendOneReg1(0x5B,0x00,0x00);
SendOneReg1(0x5A,0x00,0x00);
SendOneReg1(0x59,0x00,0x00);
SendOneReg1(0x58,0x00,0x00);
SendOneReg1(0x57,0x00,0x00);
SendOneReg1(0x56,0x00,0x00);
SendOneReg1(0x55,0x00,0x00);
SendOneReg1(0x54,0x00,0x00);
SendOneReg1(0x53,0x00,0x00);
SendOneReg1(0x52,0x00,0x00);
SendOneReg1(0x51,0x00,0x00);
SendOneReg1(0x50,0x00,0x00);
SendOneReg1(0x4F,0x00,0x00);
SendOneReg1(0x4E,0x00,0x03); //0100 1110 0000 0000 1011 1101 //Reg78 RAMP_THRESH[11]=0 QUICK_RECAL_EN[9]=0 VCO_CAPCTRL_STRT[8:1] =01011110
SendOneReg1(0x4D,0x00,0x00);
SendOneReg1(0x4C,0x00,0x0C);
SendOneReg1(0x4B,0x09,0x00); //0100 1011 0000 1001 1000 0000 //Reg75 CHDIV[10:6]= 00110=6(24)
SendOneReg1(0x4A,0x00,0x00);
SendOneReg1(0x49,0x00,0x3F);
SendOneReg1(0x48,0x00,0x01);
SendOneReg1(0x47,0x00,0x81);
SendOneReg1(0x46,0xC3,0x50);
SendOneReg1(0x45,0x00,0x00);
SendOneReg1(0x44,0x03,0xE8);
SendOneReg1(0x43,0x00,0x00);
SendOneReg1(0x42,0x01,0xF4);
SendOneReg1(0x41,0x00,0x00);
SendOneReg1(0x40,0x13,0x88);
SendOneReg1(0x3F,0x00,0x00);
SendOneReg1(0x3E,0x03,0x22);
SendOneReg1(0x3D,0x00,0xA8);
SendOneReg1(0x3C,0x00,0x00);
SendOneReg1(0x3B,0x00,0x01);
SendOneReg1(0x3A,0x10,0x01);
SendOneReg1(0x39,0x00,0x20);
SendOneReg1(0x38,0x00,0x00);
SendOneReg1(0x37,0x00,0x00);
SendOneReg1(0x36,0x00,0x00);
SendOneReg1(0x35,0x00,0x00);
SendOneReg1(0x34,0x08,0x20);
SendOneReg1(0x33,0x00,0x80);
SendOneReg1(0x32,0x00,0x00);
SendOneReg1(0x31,0x41,0x80);
SendOneReg1(0x30,0x03,0x00);
SendOneReg1(0x2F,0x03,0x00);
SendOneReg1(0x2E,0x07,0xFC); //0010 1110 0000 0111 1111 1100 //Reg46 OUTB_MUX[1:0]=00
SendOneReg1(0x2D,0xC0,0xC0); //0010 1101 1100 0000 1100 0000 //Reg45 OUTA_MUX[12:11]=00 OUT_ISET[10:9]=00 VCOOUTB_PWR=000000
SendOneReg1(0x2C,0x1F,0xA2); //0010 1100 0001 1111 1010 0010 //Reg44 VCOOUTA_PWR[13:8]=011111 OUTB_PD[7]=1 OUTA_PD[6]=0 MASH_RESET_N[5]=1 MASH_ORDER[2:0] = 010=2
SendOneReg1(0x2B,0x5F,0xD3); //0010 1011 0000 0000 0000 0000 //Reg43 PLL_NUM[15:0] =0
SendOneReg1(0x2A,0x00,0x37); //0010 1010 0000 0000 0000 0000 //Reg42 PLL_NUM[31:16] =0
SendOneReg1(0x29,0x00,0x00);
SendOneReg1(0x28,0x00,0x00);
SendOneReg1(0x27,0x61,0x99);
SendOneReg1(0x26,0x03,0x3D);
SendOneReg1(0x25,0x82,0x04); //0010 0101 1000 0010 0000 0100 //Reg37 MASH_SEED_EN[15]=1 PFD_DLY_SEL[13:8] = 2
SendOneReg1(0x24,0x00,0x20); //0010 0100 0000 0000 0010 0000 //Reg36 PLL_N[15:0] =32
SendOneReg1(0x23,0x00,0x04);
SendOneReg1(0x22,0x00,0x00); //0010 0010 0000 0000 0000 0000 //Reg34 PLL_N[18:16] =0
SendOneReg1(0x21,0x1E,0x21);
SendOneReg1(0x20,0x03,0x93);
SendOneReg1(0x1F,0x43,0xEC); //0010 0010 0100 0011 1110 1100 //Reg31 CHDIV_DIV2 =0
SendOneReg1(0x1E,0x31,0x8C);
SendOneReg1(0x1D,0x31,0x8C);
SendOneReg1(0x1C,0x04,0x88);
SendOneReg1(0x1B,0x00,0x02);
SendOneReg1(0x1A,0x0D,0xB0);
SendOneReg1(0x19,0x0C,0x2B);
SendOneReg1(0x18,0x07,0x1A);
SendOneReg1(0x17,0x00,0x7C);
SendOneReg1(0x16,0x00,0x01);
SendOneReg1(0x15,0x04,0x01);
SendOneReg1(0x14,0xE0,0x48); //0001 0100 1101 0000 0100 1000 //Reg20 VCO_SEL= 010>>VCO2
SendOneReg1(0x13,0x27,0xB7);
SendOneReg1(0x12,0x00,0x64);
SendOneReg1(0x11,0x01,0x2C); //0001 0001 0000 0001 0010 1100 //Reg17 VCO_DACISET_STRT[8:0] =100010000
SendOneReg1(0x10,0x00,0x80);
SendOneReg1(0x0F,0x06,0x4F);
SendOneReg1(0x0E,0x1E,0x70);
SendOneReg1(0x0D,0x40,0x00);
SendOneReg1(0x0C,0x50,0x01); //0000 1100 1001 0000 0000 0001 //Reg12 PLL_R_PRE[0]= 1
SendOneReg1(0x0B,0x00,0x28); //0000 1011 0000 0000 0010 1000 //Reg11 PLL_R[4]=2
SendOneReg1(0x0A,0x10,0xD8); //0000 1010 0001 0000 1101 1000 //Reg10 MULT =00001
SendOneReg1(0x09,0x06,0x04);
SendOneReg1(0x08,0x68,0x00); //0000 1000 0110 1000 0000 0000 //Reg8 VCO_DACISET_FORCE[14]=1 VCO_CAPCTRL_FORCE[11]=1
SendOneReg1(0x07,0x40,0xB2);
SendOneReg1(0x06,0xC8,0x02);
SendOneReg1(0x05,0x00,0xC8);
SendOneReg1(0x04,0x0A,0x43); //0000 0100 0000 1010 0100 0011 //Reg4 ACAL_CMP_DLY[15:8] =00001010
SendOneReg1(0x03,0x06,0x42);
SendOneReg1(0x02,0x05,0x00);
SendOneReg1(0x01,0x08,0x08);
SendOneReg1(0x00,0x64,0x1C); //0000 0000 0110 0100 0001 1100 //Reg0 VCO_PHASE_SYNC[D14]=1 FCAL_EN[]= 1 MUXOUT_LD_SEL[2]= 1
我SYNC加之前就没锁住,加了后也锁不住,同步就更不能了。
看起来您试图在full assist mode下操作LMX2594,并强制VCO_CAPCTRL_Force、VCO_DACISET_Force,这会影响设备的锁定性能。
如果想在full assist mode下使用,需要按照LMX2594数据表中的第7.3.6节使用设备,并且可以按照下面的VCO校准应用说明链接进行操作:
https://www.ti.com/lit/an/snaa336a/snaa336a.pdf
在上述配置中,如果在正常操作中使用设备(没有VCO_CAPCTRL_Force、VCO_DACISET_Force,即0),并保持MASH_order-1和PFD_DLY_SEL-1,PLL将锁定并可以看到输出。因此,可以在SYNC 功能中使用。