Other Parts Discussed in Thread: LMX2594
我测到各频点的输出功率如下图所示,可以看到整体输出频响比较平坦,1GHz到16GHz变化小于10dB,但17GHz之后功率衰减比较大,请问有什么改善方案吗?整条链路是在PLL之后又加了三级的衰减器和放大器组成。

PLL的输出部分由下图所示,采用的是电感加电阻的组合上拉方式。配置上已经enable doubler了,OUTA_PWR每个值也都试过了,并无明显改善。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
关于原理图,单端输出的话,连接方式如下图差分输出,仅需将C7右端连接改为50Ω电阻接地;(If using a single-ended output, a pullup is required, and the user can put a 50-Ω resistor after the capacitor.)
不使用的RFOUTB可以悬空,但软件需将输出配置为powered down
SYSREFREQ, RAMPCLK, 和RAMPDIR不使用的话,应该短接至GND

关于输出功率,看datasheet Figure 25.在高频段,会有一定衰减,同时也与温度有关,温度越高,输出功率越小,
8625.High Frequency Open Collector Outputs.pdf
此外,附上这个非正式的文件,深入讨论了输出功率,它是基于LMX2594的,希望对您有帮助