This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: CDCI6214 pin XOUT/FB_P 问题

Part Number: CDCI6214

Could you please help me to check which PIN ( XIN or XOUT ?) should be used as the  LVCOMOS  clock input?  

Usually , should be XIN,  But from the datasheet,  It seems that XOUT is used

  • 您好,看下引脚定义,XOUT/FB_P是LVCMOS输入引脚,没问题。XIN是crystal输入,而XOUT/FB_P是多路复用引脚,可以是crystal output,还可以是LVCMOS或者是差分输入的正相端,上图Figure3 是作为LVCMOS输入引脚。