This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214-Q1: 如何设置合理的操作模式,能用I2C把寄存器配置写入芯片(自己的板子,非EVM开发套件)

Part Number: CDCE6214-Q1

如题,我们根据参考手册的推荐电路设计了自己的硬件板子,没有使用你们的开发板和配套下载调试工具。我想使用I2C将你们的TICS-Pro配置工具生成的寄存器配置信息写入芯片,但是发现I2C操作失败。下面是我们的电路原理图:

另外,我注意到参考手册上有关于这个模式的介绍:

根据这个介绍,我理解的是要修改电路将片子的Pin4和Pin23浮空,然后进入Fall-Back Mode来使用I2C把你们上位机配置工具生成的寄存器值写入这个片子的寄存器中,然后得到我想要的输入输出。这样每次上电之后都是这个Fall-Back模式,每次都要用I2C重新配置。如果使用EEPROM,那么在进入Fall-Back时顺便将寄存器配置也写入EEPROM中,顺便再恢复Pin4和Pin23的电平状态,来进入Pin Mode或者Serial Interface Mode,这样之后上电就默认加载上一次的配置而不需要重新配置了。

那么,我的问题是:

1.我刚刚的理解是否正确?

2.如果正确,那么如果使用非Fall-Back Mode,需要事先通过I2C烧录一次配置到片子的内部EEPROM中,我在调试时还好,但这在量产的时候似乎要多一个环节?有什么办法能避免这个问题?

3.我们的电路中使用的MCU的GPIO等来控制片子的部分控制引脚,不知道有没有什么问题或者风险,你们有没有推荐的比较合适的该片子操作启动控制流程(比如可参考的伪代码之类的)?

谢谢!