Part Number: LMK04828
Other Parts Discussed in Thread: ADC12DL3200EVM,
参考adc12dl3200evm设计的,晶振输入幅值和adc12dl3200evm的晶振基本一样,但lmk04828的时钟输出幅值只有20mv.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04828
Other Parts Discussed in Thread: ADC12DL3200EVM,
参考adc12dl3200evm设计的,晶振输入幅值和adc12dl3200evm的晶振基本一样,但lmk04828的时钟输出幅值只有20mv.
您好,您的意思是使用LMK04828 作为时钟输出给ADC作为输入时钟是吗?
输入给LMK04828多大频率,欲得到多大输出频率?是如何配置的?
是的,晶振输入是100MHz,幅值大概1.6V.lmk04828七个通道都输出800MHz,但幅值只有20mv左右,datasheet上lvds的幅值大概400mv.我是先用TICS PRO进行配置导出寄存器的值然后写入lmk04828,spi读写都是正常的。
您好,7个通道输出都是LVDS信号是吗?800mV指的是VOD,也即差分输出幅值。 单端输出LVDS 400mV是没问题的。
能把您使用TICSPRo的配置页面截图看下吗?
另外,上面输出20mV的输出是什么信号,LVDS还是其他?
直接在LVDS端测量的输出吗?
如果是的话,使用差分碳棒测试的时候,请在差分输出端加上一个100ohm匹配电阻,再测试下。
另外,1.6V 100Mhz 输入,1.6V是Vp,还是1.6Vpp?因为单端输入的话,最大不超过3.1Vpp。 1.6V的话,是0~1.6V或者1.6Vpp就在范围内,如果1.6Vp就超过了输入范围。

100MHz是1.6vpp,
其实我是测的差分信号一端的峰峰值,但是adc12dl3200evm的差分信号一端的峰峰值有400mvpp,而我的只有不到20mvpp.
您好,我看电路中,输出耦合方式是采用的LVPECL的输出耦合,AC耦合电容前端使用的240ohm下拉到地。
如果您是配置的LVDS输出,耦合方式如下: