This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492: 如何使用Trig1、Trig2或者MOD管脚去触发chirp信号发射

Part Number: LMX2492


需求:想通过Trig1、Trig2或者MOD管脚给一个上升沿的触发信号,然后chirp信号开始发送,一个chirp的周期是60us,我每隔100us发送一次触发信号,就会产生一个chirp

方法:我配置MOD_PIN[2:0]为input,MOD_MUX[4:0]配置为Input MOD;start next ramp after选择 Trigger A,RAMP_TRIGA[3:0] 配置MOD terminal rising edge

问题:配置完后雷达只产生了一个chirp信号后就一直是初始值的单音信号,是我哪边的配置有问题么?

我后面把trigger1 输出MOD的状态,是一个100us一个周期的上升沿触发信号