This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: 多片LMK2594同时使用时,SPI接口如何处理?

Part Number: LMX2594
Other Parts Discussed in Thread: LMK04828,

你好,

    我的时钟树中用了1个LMK04828( CLKin_SEL0作为SDO OD模式),3个LMX2594(MUXout作为SDO),请问可以将这4个器件的SCK接在一起,SDI接在一起,SDO接在一起,然后通过CS_N选择芯片使用吗?

1.之所以问这个问题,因为我注意到LMX2594手册中有强调 The MUXout pin will always be low for the address portion of the transaction.即SPI发送地址的时候要SDO始终保持低,我不清楚这句描述是指LMX2594是否可以自己在这时保持MUXOUt输出为低,或者需要板子上其他电路强制拉这个信号为低?

2.LMK04828的CLKin_SEL0作为SDO 时明确可以配置成OD模式(CLKin_SEL0_MUX=spi readback,CLKin_SEL0_TYPE=output OD)。但是LMX2594 MUXout作为SDO时手册上未指明其输出形式,也没有找到相关配置寄存器。按一般理解OD/OC输出才可以直接接在一起,如果是推挽结构是不行的。 所以不清楚多个2594一起使用时SPI接口的SDO需要如何处理。

3.按以往的开发经验,不同器件的SPI接口SDO全部接在一起工作时时常有莫名其妙的问题,不知道TI有没有上述接法的应用验证过。

烦请答复,非常感谢。