This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208V2G: 部分频率无法配置,寻求解决方法

Part Number: CDCM6208V2G

我现在有一个用FPGA输出HDMI的板子,用的TICDCM6208V2输出HDMI的时钟,输出两个时钟,一个是像素时钟,一个serdes用的5倍频随路时钟,目前调试情况是部分分辨率的时钟能设置,有些分辨率的时钟设置不了,没法做到输出任意分辨率,比如:

1080p时钟148.5M+742.5M能设置,1280*1024分辨率的108M+540M设置不了,因为PS_APS_B只能设置成456,当随路时钟设为540M的时候不管PS_A怎么设置,VCO都不在范围内,类似的还有1024*768分辨率的65M+325M等。

我看datasheet里给的参数是最大能输出800M,请问有没有什么办法能够做到输出0~800M的任意值的。

我的硬件现在是接的一个无源晶振在SEC端,Y0~Y3输出的5倍频的随路时钟给FPGAY4~Y7输出像素时钟给FPGA