Part Number: CDCM6208V1EVM
Other Parts Discussed in Thread: CDCM6208
我的电路用的芯片是cdcm6208v1,芯片的所有供电都是3.3v,输入时钟采用第一路输入,用3.3V的25MHz单端晶振,负端用1K下拉到地,第二路时钟输入的正负都是分别用1K电阻下拉到地,采用SPI方式进行寄存器配置,所有时钟输出电压都是3.3v供电,且都采用LVDS,目前发现Y0和Y1配置成212.5M,发现实际输出只有127MHz左右
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCM6208V1EVM
Other Parts Discussed in Thread: CDCM6208
我的电路用的芯片是cdcm6208v1,芯片的所有供电都是3.3v,输入时钟采用第一路输入,用3.3V的25MHz单端晶振,负端用1K下拉到地,第二路时钟输入的正负都是分别用1K电阻下拉到地,采用SPI方式进行寄存器配置,所有时钟输出电压都是3.3v供电,且都采用LVDS,目前发现Y0和Y1配置成212.5M,发现实际输出只有127MHz左右
您好,您是使用的GUI帮助配置的吗?能否将配置页面截图看下,输入25Mhz,打算输出212.5MHz,那么配置的几个分频系数是多少? VCO频率是多少?
输出不正确,有可能分频系数配置的不当,或者不满足VCO频率范围,所以输出的值不正确。
嗯 按照这个EVM GUI配置都没问题。
您是使用的EVM还是自己的板子? 输出LVDS 测试的话,有没有在LVDS输出端接100ohm 匹配电阻测试的?还是直接在CDCM6208的输出端测试的?
建议是端接上100ohm匹配电阻再用差分碳棒进行测试。
Y7也是配置的LVDS输出吗?断开后端输出,直接在输出端测试。
Y0不正常的话,建议配置成其他频率或者其他输出格式再试试,比如LVPECL或者其他频率试试输出是否正常?
y7 也是lvds输出的,断开和不断开测试频率都是正确的,而y0其它频率也试过也是不对,但只配y0为212.5MHz其它路都disable有时是正常的,目前所有输出只配过lvds
现在把Y0和Y1配置为212.5MHz,Y2和Y3也配为212.5MHz,Y4配为108MHz,Y5配为125MHz,Y6配为148.5MHz,Y7配为200MHz;发现Y0和Y1只有127MHz左右,其他Y2-Y7的输出频率都是对的,把Y0和Y1改为LVPECL也试过,还是不正常,谢谢!我同事有个板子上的CDCM6208同样的配置情况下他的各路输出频率都是正常的,和他的板子把CDCM6208芯片做了对调,发现我的板子还是不正常。
如果是串扰的问题,请问如何解决,谢谢!