Other Parts Discussed in Thread: LMK04828, LMK04832
我们想通过LMK04828SNKDREP来实现对一个输入为100MHz的LVDS时钟信号进行分配,一共设计了5路输出,全为LVDS,100MHz的时钟信号,采用Distribution模式,电路原理图如下图所示,输入的时钟信号由一个100MHz的晶振提供,从芯片的CLKin1_P/N引脚输入,原理图上的OSCin_P/N端无信号输入。随后我们通过TICS PRO软件生成该芯片的配置信息(可见附件HexRegisterValues_distru.txt),然后再通过FPGA将所有的寄存器配置信息写入到芯片中,并回读了所有寄存器的信息,与写入的信息或者手册中的规定值一致,未发现问题,故想请各位专家帮忙看看是什么问题导致。
R0 (INIT) 0x000080 R0 0x000000 R2 0x000200 R3 0x000306 R4 0x0004D0 R5 0x00055B R6 0x000620 R12 0x000C51 R13 0x000D04 R256 0x010001 R257 0x010155 R258 0x010255 R259 0x010305 R260 0x010400 R261 0x010500 R262 0x0106F1 R263 0x010701 R264 0x010801 R265 0x010955 R266 0x010A55 R267 0x010B00 R268 0x010C00 R269 0x010D00 R270 0x010EF0 R271 0x010F10 R272 0x011008 R273 0x011155 R274 0x011255 R275 0x011300 R276 0x011400 R277 0x011500 R278 0x011679 R279 0x011701 R280 0x011801 R281 0x011955 R282 0x011A55 R283 0x011B05 R284 0x011C00 R285 0x011D00 R286 0x011EF1 R287 0x011F01 R288 0x012001 R289 0x012155 R290 0x012255 R291 0x012305 R292 0x012400 R293 0x012500 R294 0x0126F1 R295 0x012701 R296 0x012801 R297 0x012955 R298 0x012A55 R299 0x012B05 R300 0x012C00 R301 0x012D00 R302 0x012EF1 R303 0x012F01 R304 0x013002 R305 0x013155 R306 0x013255 R307 0x013300 R308 0x013400 R309 0x013500 R310 0x013679 R311 0x013700 R312 0x013840 R313 0x013900 R314 0x013A0C R315 0x013B00 R316 0x013C00 R317 0x013D08 R318 0x013E03 R319 0x013F00 R320 0x0140F7 R321 0x014100 R322 0x014200 R323 0x014391 R324 0x014400 R325 0x014500 R326 0x014610 R327 0x014733 R328 0x014802 R329 0x014942 R330 0x014A02 R331 0x014B16 R332 0x014C00 R333 0x014D00 R334 0x014E00 R335 0x014F7F R336 0x015003 R337 0x015102 R338 0x015200 R339 0x015300 R340 0x015478 R341 0x015500 R342 0x015696 R343 0x015700 R344 0x015896 R345 0x015900 R346 0x015A78 R347 0x015BD4 R348 0x015C20 R349 0x015D00 R350 0x015E00 R351 0x015F0E R352 0x016000 R353 0x016102 R354 0x01625D R355 0x016300 R356 0x016400 R357 0x01650C R369 0x01710A R370 0x017200 R380 0x017C15 R381 0x017D33 R358 0x016600 R359 0x016700 R360 0x01680C R361 0x016959 R362 0x016A20 R363 0x016B00 R364 0x016C00 R365 0x016D00 R366 0x016E16 R371 0x017320 R386 0x018200 R387 0x018300 R388 0x018480 R389 0x018500 R392 0x018800 R393 0x018900 R394 0x018A00 R395 0x018B00 R8189 0x1FFD00 R8190 0x1FFE00 R8191 0x1FFF53