Part Number: LMK05318
使用芯片LMK05318,参考输入1PPS,目标输出1PPS和6路2MHz时钟与参考输入同步。参考1PPS来自GPS接收模块。目前测试发现输出的PPS与输入参考PPS的同步速度非常慢,完全实现相位同步可能需要数小时。请问在TICS Pro中怎样设置,可以加快同步的速度,实现几分钟之内相位同步?可以接受同步过程中输出频率的偏差,但要求相位快速同步。附件是我这次的使用的配置文件,请问这样的配置是否有问题?7457.同步采样时钟配置-LMK05318-0316.tcs


你好,我按照你给的建议设置了,但是我发现,当我勾选SYNC_SW以后,输出会消失,但是不勾选就有输出,请问这是为什么?应该如何解决?(此时ZDM已经勾选)