This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: 关于自动跳频时的设置

Part Number: LMX2595


 您好,正在进行验证LMX2595的自动跳频功能的验证。关于数据手册上的这部分有些看不懂的地方。请问ramp_length是什么参数呢?以及示例表格中的计算1000x50MHz,这个1000是什么参数呢?感谢您的回答。

  • ramp_length:  The user programs the length of the ramp in phase detector cycles.指的是用户在相位检测器周期中对扫频的长度进行配置。

    我们可以根据表格上面的举例来理解:

    Suppose user wants to generate a sawtooth ramp that goes from 8 to 10 GHz in 2 ms (including calibration breaks) with a phase-detector frequency of 50 MHz. Divide this into segments of 50 MHz where the VCO ramps for 25 µs, then calibrates for 25 µs, for a total of 50 µs. There would therefore be 40 such segments which span over a 2-GHz range and would take 2 ms, including calibration time.

    也就是说,假设我们要在 2ms 内从 8GHz 到 10GHz 的锯齿扫频 (包括校准) ,相位检测器频率为 50MHz,按照这50Mhz分成段,而VCO扫频时间为25us,校准时间为25us,一共50us扫频一次。

    因此50Mhz的VCO频率,要扫2Ghz频率,至少需要2G/50M=40段, 也就是需要40*50us=2ms完成扫描。

    ,。 

     

  • 您好,感谢您的回答。我看到tics上的默认配置这里也是乘以1000,请问我可以将这个1000理解为每个频点的配置时间吗?

    另外还想向您请问跳频步进的计算式那里,以数据手册中的示例为例,为什么有一个除以50000的算式?

    期待您的回复,感谢。

  • 请问我可以将这个1000理解为每个频点的配置时间吗?

    可以理解成每个频点的扫频时间。 那么50Mhz需要的时间即为50000.

    而ramp increment指的是相位检测周期内ramp0或1的递增量,

    而ramp-length,即50000指的是相位检测器周期中扫频的长度。

    所以除以50000是不是可以理解为扫频的步进量。 

    不知这样解释是否能理解,对于这个表格里的定义和式子,我也是看到这个公式一点点的去推断和理解的,实际用的时候一般也都是通过TICSpro去帮助配置的。 

    如果还有什么问题,大家再一起讨论。

  • 您好,感谢您的回答。您的回答帮助我理解了很多。但是还有一个点有些不解想向您请教。您说50000表示的是一个相位检测周期的扫频长度(单位微秒),而表格中计算ramp_inc的计算式为(2000 MHz) / (50 MHz) × 224 / 50000 = 13422,即是用分段数的值40除以50000,这个值为什么可以看成是扫频的步进量呢?期待您的回复,感谢。

  • 您好,2000Mhz除以50Mhz,指的是扫频带宽中有40段50Mhz的频段,而每个50Mhz又有50000个扫频长度。 在这个50Mhz的相位周期里一共有50000个扫频长度,所以除以50000是不是可以理解为扫频的步进量。 

  • 感谢您这么多次的耐心解答,在您的帮助下我已经完全理解了。十分感谢。

  • 不必客气, 后续有什么问题大家一起讨论。