Part Number: LMX2595
您好,我试图将四片LMX2595芯片的输出进行同步合成。由于硬件设计上的问题,需要对其中一片的相位进行调整。在进行相位调整时,出现了如下的问题:当未进行相位调整的芯片进行合成时,其谱线很正常。
而当我将其中一路LMX2595的相位通过mash_seed微调时,出现了下面的情况:在每0.5MHz的偏移处会出现很糟糕的杂散。
请问出现这种情况的原因是什么呢?会是因为使用mash_seed功能而出现了小数分频杂散吗?如果是因为小数分频杂散,请问LMX2595如何在不引入小数分频杂散的情况下实现相位调整呢?
下面是我的环路滤波器设置以及主要寄存器设置(调整mash_seed为660时)