您好!
我在CDCM9102 规格书上看到下面电路, 但是我不清楚 VDD 应该用多少V 电压
我这边设计是一个 PCI-E Gen3 产生一个HCSL的100M CLK 时钟, 麻烦你告知我一下 谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,VDD即为CDCUN1208这颗时钟缓冲器的供电电压1.8V(可以参考CDCUN1208的datasheet:https://www.ti.com.cn/lit/ds/symlink/cdcun1208lp.pdf)。 这里CDCM9102输出和CDCUN1208的输入AC耦合,通过上下拉电阻分压电路重新建立新的共模电压。
根据您的应用,可以这样设计,CDCM9102输出LVPECL电平,通过recevier来得到HSCL 电平输出的目的。 即下面这个应用。但是CDCUN1208是多路输出的,是个扇出缓冲器,我找了下单路的,好像没有单路的。