This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用CLKIN0 作输入,输入为61.44MHZ 时,LOCK灯是亮,把频率改为30.72MHZ,同步修改RDIVIDER 值,为什么无法锁定,对CLKIN0 的频率有严格要求吗
另外:PLL2的锁定和输出频率与PLL1的锁定与否没关系是吗,CLKIN0的输入频率并不影响板上EXTVCO的运行对吗,也就是说不管CLKIN0频率多少或者是否稳定,EXTVCO 都是正常运行的,对吧
配置参数
输入时钟波形
评估板
您好,CLKIN的频率范围为0.001~750Mhz,在这个范围内都可以。
输入改成30.72Mhz之后,打算输出频率是多少? 不能lock可以看下是不是不在VCO频率范围之内。
PLL2的锁定和输出频率与PLL1的锁定与否没关系是吗
是的,有时候PLL1能正常锁定,有时候PLL2能正常锁定。
external VXCO是OSCin的输入。或者说OSCin的输入来自于crystal或者VXCO。