This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492: TRIG1、TRIG2、MOD、MUXout作用是什么

Part Number: LMX2492

你好,我在使用LMX2492的时候遇到了困难,我不太清楚TRIG1、TRIG2、MOD、MUXout,这几个引脚的作用是什么,定义是什么,因为数据手册上也没有这几个引脚的定义和推荐配置,我如果想要只设置一个简单的ramp,就跟数据手册里的例子一样(例子里没有这几个引脚的推荐设置),我该如何选择他们

  • 您好,数据手册上Page3有对各个引脚的定义呢:https://www.ti.com.cn/lit/ds/symlink/lmx2492.pd

    这几个引脚的配置,可以参考Table6,使用引脚配置或者寄存器,比如:

    通过寄存器R36 bit【2:0]=001,说明TRIG1这个引脚是个OD输出引脚,默认配置下为三态。Table6说明的是TRIG1,TRIG 2和MOD,MUXOUT这几个引脚的状态。

    而Table7 则说明的是这几个引脚经过MUX的状态:比如R36[7:3}=00001,MUX状态为Input triger1.然后按照table8的寄存器配置,RAMP_TRIGA如果配置为1,则trigger信号为上升沿触发。我理解的就是扫频时的触发信号,比如每100us扫频一次,则每100us发一个触发信号给Trig1.

  • 您好,还想再麻烦您一下,我网上下载了一个例程,它将TRIG1_PIN、TRIG2_PIN=7(也就是input),MOD_PIN、MUXout_PIN = 0(defalut),TRIG1_MUX=

    3(input MOD),TRIG2_MUX = 1(input TRIG1)  ,  MOD_MUX、MUXout_MUX = 0(GND)。这样配置的话,会有什么效果,是不是意味着TRIG1、TRIG2、MOD三者是不是就一样了,如果此时我将Ramp_CLK = 1 (MOD  source),会有什么效果?

     

    感谢您百忙之中解答

  • 它这个配置的意思是,TRIG1和TRIG2 为输入引脚,TRIG1 输入的是MOD 信号,TRIG2 输入的是TRIG1的输入。

    MOD引脚和MUXout 引脚为GND状态。

    所以如果Ramp_CLK = 1, 我的理解是需要MOD_MUX=3, 为input MOD。 TRIG1_PIN、TRIG2_PIN可以配置为三态,TRIG1_MUX=1 input TRIG1.

    TRIG2_MUX=2,input TRIG2.

    建议您在使用时钟器件进行配置时,使用TICSPro tool帮助进行配置。