This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: 在所需15.4-16.4GHz RAMP输出附近,有很多杂波出现

Part Number: LMX2595

TICS PRO配置如下:

在所需频端周围出现很多杂波,测试窄带频谱图(Max Hold)和全频带频谱图如下:

修改 Desired Duration,没有很大的效果。

1. 请问是什么原因导致的呢?

2. 请问有何改进方法?

非常感谢!

  • 您好,

    为更加有效地解决您的问题,我将您的问题发布在了E2E英文论坛上,将由资深的英文论坛工程师为您提供帮助,请等待帖子的回复,帖子链接:

    https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1098854/lmx2595-near-the-required-ramp-output-15-4-16-4ghz-there-are-a-lot-of-clutter

  • E2E工程师已回复:

    You are sweeping the VCO frequency between 7700MHz and 8200MHz, the sweep range is 500MHz, as such, multiple VCO calibrations are required during sweep. You have setup VCO calibration every 100MHz sweep, this setup should be ok but you did not setup enough time for the calibration. Suggest put at least 50µs in the Min. VCO Calibration Time field. 

    Since multiple VCO calibrations are required in order to support 500MHz sweep, the sweep is not a linear frequency sweep. If you are looking for linear sweep, we have to limit to sweep range to around 100MHz. 

    The RST bit is not needed as the end frequency of RAMP1 is equal to the start frequency of RAMP0.

    对应的中文是:

    您正在扫描7700MHz 和8200MHz 之间的 VCO 频率,扫频范围为500MHz,因此,扫频期间需要多个 VCO 校准。 您每扫描100MHz 就设置一次 VCO 校准,此设置应该可以,但您没有为校准设置足够的时间。 建议在Min VCO Calibration Time 中至少加50µs。

    由于支持500MHz 扫描需要多个 VCO 校准,因此扫描不是线性频率扫描。 如果您正在寻找线性扫描,我们必须将扫描范围限制在100MHz 左右。

    不需要 RST 位,因为 RAMP1的结束频率等于 RAMP0的开始频率。

  • 你可以配合THRESHOLD和RAMP_TRIG_CAL进行优化,使得频率参数在小范围改变而较稳定。desired duration可以按照TICS推荐(可以设置大一点TICS会自己推荐值)。

  • 你好,按照昨天TI工程师的建议,我设置了50us的VCO校准时间,发现并没有很大改善。昨天通过仪器的transient analysis观察了波形,发现主要原因是在VCO校准时有比较大的杂散出现,因此想通过降低鉴相频率和threshold(皆为50MHz),通过多分段(也就是您说的那个意思)来改善,测试结果如下,也没多少改变。接下来准备尝试 1.通过RAMP_TRIG_CAL来优化;2.增大环路滤波器带宽。

  • 你好,问一下图片和视频怎么插入,我的无法插入,没法直观表现。

  • 如果用电脑的话,可以直接把图片和视频拖到网页的界面上传的。

  • 你好,没太理解您视频的意思,还麻烦您指教一下

  •  是这样的要求吗?

  • 你好,我的带宽是500M*2,从15.4-16.4GHz,好像和您测得不太一样呀

  • 发现在开始校准时会有如图所示的毛刺出现,经观察,毛刺频率为所用VCO核VCO1的上下边界,即7.5GHz和8.6GHz。请问毛刺产生的原因是什么,有何有效解决措施呢?非常感谢!

  • 第一个视频是15.4-16.4GHz,后面的是为了显示直观。

  • For waveforms that are NOT calibration free, the slew rate of the ramp must be kept less than 250 kHz/µs. Also,
    for all automatic ramping waveforms, be aware that there is a very small phase disturbance as the VCO crosses
    over the integer boundary, so one might consider using the input multiplier to avoid these or timing the VCO
    calibrations at integer boundaries.

  • 哦哦, 这样子。想请问您是怎么设置TICS PRO的呢,非常感谢!

  • RAMP_TRIG_CAL来优化

  • 感谢 jia zhou的分析!如果后续您有什么疑问,您也可以直接在E2E英文论坛(上面链接)回复帖子,或者发布在这里,我会转发至E2E英文论坛

  • 您好,不好意思,我看您的设置扫描频率是7700-7730MHz,不是我对应的7700-8200MHz呢。而且使能RAMP_TRIG_CAL功能,貌似没有太大的改进。

  • 你把7730MHz改成8200MHz就行了,RAMP_TRIG_CAL打开再关闭,观察没有其他调谐杂散后最终是关闭的。

  • 您好,我已将您的这个问题发布在了E2E英文论坛上,也给出了相应的论坛链接,请等待E2E论坛工程师的回复

  • 因为您长时间未回复帖子,我们认为您的问题已解决,若还有疑问,请回复帖子