每个LMX2594芯片是否有它的唯一性,在使用全辅助模式校准VCO时,寄存器R20、R19和R16的值是否都需要重新回读得到?如果将回读的寄存器的值写入到另一个LMX2594芯片中,会发生什么问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
每个LMX2594芯片是否有它的唯一性,在使用全辅助模式校准VCO时,寄存器R20、R19和R16的值是否都需要重新回读得到?如果将回读的寄存器的值写入到另一个LMX2594芯片中,会发生什么问题?
您好,每个芯片在初始状态下的寄存器都是默认值,需要根据不同的应用去进行配置。
像您说的,回读的寄存器写入另一个LMX2594中,那就相当于对另一个LMX2594的寄存器进行配置。
不知是否误解了您的意思,芯片是唯一性的,对一片LMX2594进行读写,跟另一片LMX2594没有关系。
对于快速跳频的应用,我们需要提前将需要频率的R20,R19和R16回读出来存成表格,后面跳频的时候只需要直接按照对应的关系写寄存器。我的疑惑是:是不是每个芯片都需要做这个回读的工作?如果我将回读得到的数据应用于任何一个LMX2594芯片是否可以正常工作?
回读的话配置MUXOUT_LD_SEL=0来对MUXOUT的输出引脚状态来判断对芯片配置或者锁存状态,回读的作用如下。 当然您也可以不进行回读,所以您若直接将回读的数据写到另外一片LMX2594中是没有意义的,它并不代表这片LMX2594的比如PLL是否锁存,VCO一些校准信息,配置是否正确等。 所以还是像您说的,需要实际验证,进行troubleshoot。