Part Number: LMX2594
PFD_DLY_SEL寄存器的作用是什么?手册只写如何设置并没有解释功能。
假设我们设置MASH_ORDER=3,PFD_DLY_SEL为3。
当设置输出频率变化时,根据表2,如果fvco >10000mhz,需要PFD_DLY_SEL =4,
但是我仍保持PFD_DLY_SEL为3,会有什么结果?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2594
PFD_DLY_SEL寄存器的作用是什么?手册只写如何设置并没有解释功能。
假设我们设置MASH_ORDER=3,PFD_DLY_SEL为3。
当设置输出频率变化时,根据表2,如果fvco >10000mhz,需要PFD_DLY_SEL =4,
但是我仍保持PFD_DLY_SEL为3,会有什么结果?
您好,PFD_DLY_SEL参考Table2 是芯片研发工程师根据理论值得到的最佳相位噪声的结果,是个理论上的值。
实际应用时,可以根据Table2中推荐的上下浮动1,确认配置哪个值的相位噪声最好就采用哪个。
意思是
如果fvco >10000mhz,需要PFD_DLY_SEL =4,但是我仍保持PFD_DLY_SEL为3。
这样做并没有什么影响,只是稍微影响一些相位噪声?
是的,主要影响了相位噪声,这个是芯片设计者给出的理论值,实际应用中上下浮动1配置都是可以的,可以对比下配置为3和4的总体性能,哪个好就使用哪个值。