CDCLVC1112输入用信号源输出的10MHZ 3.3vpp的正弦波,芯片输出引脚没有波形输出。将信号源输出的波形经过交流放大放大电路,交流放大电路加了偏置,再输入CDCLVC1112,芯片输出是有波形的。因放大电路输出波形有失真,1112输出端的波形也是失真的。
请问,以上信号源输出的10MHZ正弦波直接输入到1112为什么会没有输出呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CDCLVC1112输入用信号源输出的10MHZ 3.3vpp的正弦波,芯片输出引脚没有波形输出。将信号源输出的波形经过交流放大放大电路,交流放大电路加了偏置,再输入CDCLVC1112,芯片输出是有波形的。因放大电路输出波形有失真,1112输出端的波形也是失真的。
请问,以上信号源输出的10MHZ正弦波直接输入到1112为什么会没有输出呢?
CDCLVC1112输入用信号源输出的10MHZ 3.3vpp的正弦波,芯片输出引脚没有波形输出
3.3Vpp是+-1.65V还是0~3.3V的信号?加了偏置之后能正常输出,说明输入信号满足它的输入电压范围。之前没加偏置,不能输出很大原因是输入范围不满足下面的要求。

输入是正负1.65的正弦波。
不加偏置不行是不是112不能识别负幅值呢
是的。112不能识别负值信号。 供电电压也是单电源供电,3~3.6V,典型值为3.3V。
输入信号的最大幅值范围0~VDD。
您好,是这样,我又测了一下加偏置输入10MHZ的正弦波,输入是0-3.3V,发现经过1112后,输出是方波,而且频率低的方波更明显,频率加大(我这边信号源只能到20MH),输出有正弦波趋势。请问,这个有可能是什么问题呢?我看1112规格书上频率能到200多MHZ的