Part Number: LMH7322
开发板前端,给了一个1MHz的方波,然后测试第一级输出的LVDS信号,使用普通探头,一端接地,一端分别测试匹配电阻R2两端,始终测不到波形,请问应该怎么测试,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH7322
开发板前端,给了一个1MHz的方波,然后测试第一级输出的LVDS信号,使用普通探头,一端接地,一端分别测试匹配电阻R2两端,始终测不到波形,请问应该怎么测试,谢谢。
搜索
复制
开发板前端用示波器给了一个1MHz,0-3V的方波。然后使用单端探头和差分探头测量第一级模拟转LVDS的输出端匹配电阻R2两端的电压,但是开发板此处电压时钟保持一条直线,高电平是1.5V,低电平是-0.2V。原本以为是自己测试方法或者设备有问题,但是同样方法去测试一个标准LVDS信号输出,压差,波形测试都是正常的。所以想请问这个板子的第一级输出端信号有什么特别的方法吗,这个开发板是2.5V和-5.2V供电,求教,谢谢。
搜索
复制
输入0-3V的方波可能已经损坏了比较器,决对最大额定值电压输入范围是VEE-0.2V ~VCCI+0.2V,EVM板VCCI是2.5V,输入3V已经超过这个范围:

电气特性要求的范围如下蓝色框内:

您可以登录 LMH7322 主页,如下链接,点击网页右上角的“立即订购”,会出现如下截图, 看是否可以申请样片,然后换上EVM板上的LMH7322,以解决问题
https://www.ti.com.cn/product/cn/LMH7322

您好,之前没有测到波形是因为S1拨码开关的选择导致第一级输出终止。现在第一级是有输出了,前端模拟信号给了一个+-1V , 1MHz的方波,VCCA 2.5V VEE -5.2V,正常按照手册高低电压应该为VCCA-1.1和VCCA-1.5 。但是实际测得一端对地电压为1.5V,另一端则为-0.2V,请问为什么会出现这样的情况?谢谢
搜索
复制
S1拨码开关只是用来锁住输出,使其输出保持住,对输入过压并没有影响,因此,我怀疑您在输入0-3V的方波时可能已经损坏了比较器造成的,建议换一个LMH7322芯片再做测试