This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04821EVM: CS1241965,LMK04821EVM的使用

Part Number: LMK04821EVM

Hi, Dear,

We use LMK04821EVM to evalute  our application, that need 10MHz clock(Using A Rubidium Oscillator) as input reference clock, not use default 122.88MHz clcok.

When we using default 122.88MHz clcok as input clock to OSCIn, the PLL2 show can locked.

But we try switch to 10MHz clock as input to OSCIN, Single PLL. We cann't config the EVB to locked.
So, is there any suggestion or guidance to our seeting?  Thanks a lot~

The attached configue:

Input clock: 10MHz, Output Clock:1000MHz,Using VCO1=3000MHz.