Part Number: CDCE62005
数据手册显示fan-out mode时,CDCE62005可以输出最大1.5GHz?想咨询下,如果需要输出1.25GHz的频率,是否需要输入1.25GHz的时钟?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCE62005
数据手册显示fan-out mode时,CDCE62005可以输出最大1.5GHz?想咨询下,如果需要输出1.25GHz的频率,是否需要输入1.25GHz的时钟?
您好,
数据手册显示fan-out mode时,CDCE62005可以输出最大1.5GHz?
如果divider=1即divider bypass的话,输出最大为1.5Ghz。
fanout模式下,如果分频系数为1(即divider bypass mode),那输入输出频率是相同的,只是做buffer。所以参考下图,bypass mode下的频率范围能达到1.5G,如果使用分频功能的话,输入频率最大1.175GHz。 所以如果您需要输出1.25Ghz的话,如果使用divider bypass mode,输入也需要1.25GHz.