This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: CDCE62005是否可以同时产生1.25GHz、62.5MHz、33MHz?

Part Number: CDCE62005


CDCE62005是否可以同时产生1.25GHz、62.5MHz、33MHz(或者33.333MHz)?

  • 您好,建议安装CDCE62005 software。然后将输入输出频率填写进去,会自根据分频系数和VCO频率的范围自动得到输出,看是否能得到这几个精确的输出频率。

    我今天下午试了试这个软件,电脑一直安装不上,应该是我电脑的问题, 您看下是否能正常安装?