This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: LMX2820,PFD IN管脚的DC电压怎么是3.2V

Part Number: LMX2820

请问LMX2820,PFDIN管脚的DC电压怎么是3.2V而不是像RF IN或者OSC IN那样是偏置在1.6V?像是被禁止了,

是需要设置R57(0)=0,然后写R0后才会正常吗?

实际这样操作后仍无法改变。

将LMX2820当成一个低噪声pll用时,即:用外部VCO,外部混频,PFD IN输入,

这时的寄存器配置是怎样的呢?

设置为EXT VCO模式吗?

这种模式下,配置寄存器有顺序吗?

谢谢

  • 请问LMX2820,PFDIN管脚的DC电压怎么是3.2V而不是像RF IN或者OSC IN那样是偏置在1.6V?像是被禁止了,

    您好,您测试下来PFDIN的偏置电压为3.2V是吗?您是怎么测试的,给了一个交流信号发现偏置电压3.2V还是悬空测量的?

    关于寄存器配置顺序问题,LMX2820我查了下,没有寄存器配置顺序的需求,如果有些寄存器的默认值和需要配的值一样,则不用管这个寄存器。只配一些需要配置的寄存器即可。

    可以使用TICSPro帮助配置。