在使用过程中对该时钟芯片有如下几点疑问,麻烦帮忙回答:
1、LDO34是给OUTPUT0、3、4供电,为什么寄存器R4的bit7-6是如何控制上电下电?在调试的过程中发现00、01out0有输出,01,11没有输出;
2、R25的bit10的作用是enable clock mux to Y0,Y0是什么呢?手册里面没有相关描述。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用过程中对该时钟芯片有如下几点疑问,麻烦帮忙回答:
1、LDO34是给OUTPUT0、3、4供电,为什么寄存器R4的bit7-6是如何控制上电下电?在调试的过程中发现00、01out0有输出,01,11没有输出;
2、R25的bit10的作用是enable clock mux to Y0,Y0是什么呢?手册里面没有相关描述。
R25的bit10的作用是enable clock mux to Y0,Y0是什么呢?手册里面没有相关描述。
Y0即为OUT0,指的是参考输入时钟在PLL bypass条件下的输出频率。
可以借助于TICSPro的架构图来看,便于理解。
LDO34是给OUTPUT0、3、4供电,为什么寄存器R4的bit7-6是如何控制上电下电?在调试的过程中发现00、01out0有输出,01,11没有输出;
我没太明白您这里的意思,VDDO_34是output0,3,4通道输出的供电电压。 R4的bit7,6是如何控制上电掉电是什么意思?
R4的bit7和bit6分别是enable和disable CH3和CH4的LDO,另外,调试中00,01,OUT0有输出,指的还是R4的bit7:6的配置吗?
如果是的话 ,配置为00,01,OUT0有输出,配置为01,11没有输出也是OUT0吗?