Part Number: LMK5C33216EVM
Other Parts Discussed in Thread: LMK5C33216
1-PPS输入对应的配置寄存能不能提供1份HexRegisterValues.txt,开发板没有1-PPS和ZDM相关的默认配置,DS中相关介绍比较少,使用起来相对困难。
尝试过1-PPS从REF0输入,作为DPLL2的参考;DPLL2 ZDM from OUT0(从SYSREF输出1Hz的时钟信号)。过程中主要碰到3个问题:
1、将DPLL2_REF0_RDIV和DPLL2_FB_DIV均设置成10,也就是DPLL的鉴相器频率为100mHz,但是配置完之后发现APLL2和DPLL2配置出来对应的VCO2频率不一致;
2、对于1Hz的REF0检测该怎么配置,1Hz的方波和正弦波从REF0给进去都尝试过,但是回读状态里面REF0_VALID_STATUS=0;
3、1-PPS输入对应的芯片的配置步骤,麻烦介绍一下;