Part Number: LMX2594
Other Parts Discussed in Thread: LMX2572
使用LMX2594能否进行FSK调制,实现两个频率点的跳频,需要通过配置哪些寄存器完成,麻烦给个参考样例和计算样例。
也就是实现2572中的FSK功能,但是由于项目需要,只能使用2594,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我已向资深的英文论坛工程师确认这个问题,请耐心等待回复:
LMX2594不像LMX2572那样包含FSK 引擎。
LMX2594仍然可以实现FSK。
如果您只需要离散2FSK调制,您可以使用Manual ramping 功能并切换RampDir引脚。
如果您需要像GFSK这样的shaped-FSK 调制,那么您需要连续编程N分频器,类似于LMX2572的FSK SPI模式。
LMX2594 does not contain the FSK engine like LMX2572.
FSK is still possible with LMX2594.
If you only need discrete 2FSK modulation, you can use the Manual ramping function and toggle the RampDir pin.
If you need shaped-FSK modulation such as GFSK, then you need to continuously program the N-divider, similar to LMX2572's FSK SPI mode.