即时校准的锁定时间问题
我使用TICS Pro模拟即时校准,并用示波器抓取TP_LD的低电平脉冲宽度
TICS Pro采用以下推荐的配置流程,流程来自于链接回复:LMX2820: LMX2820 not locking with instant calibration - Clock & timing forum - Clock & timing - TI E2E support forums
After a Vcc power up, we need to program the device to lock to a certain frequency without InstCal (INSTCAL_EN=0). After the device is locked, then we can initiate the InstCal.
Recommended programming sequence below:
- Open TICS Pro and select EVM default mode configuration
 - In User Controls page, check all Double Buffer bits
 - In PLL page, uncheck DBLR_CAL_EN in Instant calibration box (if VCO doubler is not needed)
 - Vcc power up the EVM
 - Press Ctrl+L to program the EVM to lock to 6GHz
 - Set INSTCAL_EN = 1 in Instant calibration box
 - Type 5650 and then Enter in the VCO box (PLL_NUM, PLL_N and INSTCAL_PLL_NUM will be programmed automatically)
 - Uncheck FCAL_EN in the VCO calibration box
 - Check FCAL_EN
 - Uncheck FCAL_EN and wait for a while (VCO will lock to 5650 MHz), InstCal is complete.
 - Change VCO frequency, for example, type 5800 and then Enter in the VCO box (PLL_NUM, PLL_N and INSTCAL_PLL_NUM will be programmed automatically)
 - Click Calibrate VCO button (this will write R0 once, VCO will lock to 5800 MHz)
 - Change VCO frequency to 6200 MHz
 - Click Calibrate VCO button (this will write R0 once, VCO will lock to 6200 MHz)
 
在VCO与VCO Divider模式下,即时校准的跳频锁定时间在6-7us之间,但手册给出的即时校准时间为2.5us,在VCO Doubler 模式下,跳频锁定时间在60-70us之间
- 为什么即时校准的锁定时间会超过5us,中间是包含了稳定时间吗?
 - 为什么使用输出倍频器后,锁定时间明显的变长了?是需要进行其他操作吗?