Part Number: CDCE62002
Other Parts Discussed in Thread: CDCE62005
我们使用CDCE62002设计一款产品,经过一段时间的验证,常温应用环境都正常,但是现在在一种情况下出现了问题。我们在低温-40℃情况下给设备加电,将CDCE62002配置成功后,其功能正常,然后给设备升温,速率约为10℃/h,在芯片的环境温度65℃左右时(个别设备温度可能再偏高一些),某些设备会出现失锁的情况,芯片配置输出为单通道1024M。
后续我们将每次都出问题的设备和每次都不出问题的设备上的CDCE62002互换,然后设备的现象也互换了,所以我们分析可能故障和芯片本身有一些联系,不知道您有没有相关的线索。期望收到您的答复。