Part Number: LMK04821
在调试过程中,发现OSCIN没有时钟输入的时候,LMK04821依然有时钟输出,这个现象正常吗?恢复250M的时钟后,JESD204B出现建链异常的问题。
主要的疑虑是:为什么没有时钟输入的时候,LMK04821仍然有频率输出?会有轻微频偏。
正常输入250MHz时钟后,jesd204B通信反而出现问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04821
在调试过程中,发现OSCIN没有时钟输入的时候,LMK04821依然有时钟输出,这个现象正常吗?恢复250M的时钟后,JESD204B出现建链异常的问题。
主要的疑虑是:为什么没有时钟输入的时候,LMK04821仍然有频率输出?会有轻微频偏。
正常输入250MHz时钟后,jesd204B通信反而出现问题?
您好,
CLKin管脚有输入吗?您是使用的EVM板吗? 输出是什么?您是使用的哪个配置工具(CODELOADER or TICSPRO)配置的 LMK04821?您是怎样配置的?或者说您的应用是怎样的?
PLL1才有holdover功能,我也很奇怪外部时钟输入断开后,PLL2的VCO为什么还是有输出的,这一点我再看下datasheet;
低温的时候,发现VCO的频率会偏
低温的时候,信号源频率是否有改变?