Part Number: LMK05318B
Hi,
I have some questions about the synchronization capabilities of LMK05318B devices.
When I use the 1pps clock of GPS as a reference input, there are several questions that I don't understand all the time
1. OUT7 of 05318B has ZDM function, so only the phase of OUT7 can be consistent with the input PPS phase?
2. What is the relationship between the phase of out0~6 and the phase of PPS? What is the relationship with the phase of out7?
3. When I use the ZDM function to synchronize out7 to PPS, and then use the sync function to synchronize all output clocks, after synchronization, what is the phase relationship between out0~6 and out7?
4. Which reference is the sync synchronization function to synchronize the phase of each channel to? Can I synchronize the phase of out0~6 to out7?