Part Number: LMX2820EVM
Other Parts Discussed in Thread: LMX2820
HI Team
1. 请问LMX2820即时校准的原理是什么?
我现在可以使用即时校准的方式进行跳频,但是我不理解即时校准锁定的原理
2. 请问LMX2820相位同步的原理是什么?我想更加深入了解一下
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2820EVM
Other Parts Discussed in Thread: LMX2820
HI Team
1. 请问LMX2820即时校准的原理是什么?
我现在可以使用即时校准的方式进行跳频,但是我不理解即时校准锁定的原理
2. 请问LMX2820相位同步的原理是什么?我想更加深入了解一下
谢谢
您好,
1、下面文档希望对您有帮助:
Dramatically Improve Your Lock Time with Vco Instant Calibration (snaa342)
也有对应的中文版:通过 VCO 即时校准显著缩短锁定时间
2、下面链接指南中,介绍了相位同步的原理,相位同步的局限性,并演示如何设置同步。
我咨询了美国的工程师,他的回复:
Details of calibration is here: https://www.ti.com/lit/pdf/snaa336
Phase synchronization is used to maintain a deterministic latency between output and input.

After synchronization, the latency is not zero and varies from part to part. As a result, the output phases from multiple devices will not be exact.
翻译如下:
校准的详细信息:https://www.ti.com/lit/an/snaa336a/snaa336a.pdf
相位同步用于保持输出和输入之间的确定性延迟。

同步后,延迟不是零,并且因部分而异。 因此,多个设备的输出相位将不准确。
完全辅助需要手动生成LUT并进行应用,而这两项操作都是在即时校准中自动执行的。 此外,即时校准将使用寄存器双缓冲,输出频率不会改变,直到应用LUT。
Full assist requires LUT generation and application manually while both of these operations are automatic in Instant calibration. In addition, instant calibration will use register double buffering, output frequency won't change until LUT is applied.