This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: VCO_2X后高频段输出较小,而VCO输出较大

Part Number: LMX2595


OUTA输出19G输出大小为-55dBm,但是频谱仪上9.75G的VCO输出为-10dBm左右,请问,我需要 15-20G频段输出,还需要设置什么?已开VCO_2X和EN=1

  • 您好,

    您是使用电阻上拉吗?您可以配置 OUTX_PWR寄存器来获得可能的最高输出功率,使用电感上拉也可以增加输出功率。

    输出 15-20G频段需要将寄存器DBLR_IBIAS_CTRL1  设置为0x0C2B,在datasheet 8.1.5章节有不同设置下的曲线对比图,您可以看下。

    另外,这么高频率的输出,PCB布局非常重要,请尽量缩短元件间距离和PCB走线。

  • 谢谢你,我已解决。失误将寄存器操作复位了。