CDCLVC1112使用3.3V供电,分别输入5dbm和10dbm正弦波,输出通道Y0使用分压电阻想将3.3V时钟分压成1.8V时钟,使用100Ω和120Ω搭配,但示波器测量Y0通道输出只有1.92Vpp,分压后只有1.08Vpp,为什么输出的波形不是3.3V呢?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1112使用3.3V供电,分别输入5dbm和10dbm正弦波,输出通道Y0使用分压电阻想将3.3V时钟分压成1.8V时钟,使用100Ω和120Ω搭配,但示波器测量Y0通道输出只有1.92Vpp,分压后只有1.08Vpp,为什么输出的波形不是3.3V呢?


您好,电路没有问题,5dbm和10dbm正弦波输入输出都是只有1.92Vpp吗?输入端在靠近引脚端的波形测试了吗?是否是3.3V?
检查下是不是焊接的问题?
有量过,进入芯片的波形和与单独测量5dbm和10dbm的波形是一样的。
是输出是1.92Vpp,输入是正常的5dbm和10dbm。
是的,您这里是建立1.65V的直流分量了,那也就是说0~3.3V的正弦波输入,输出只有0~1.92Vpp。
电路没有问题,有没有测试下Y1输出是否正常?
Y1是正常的,就Y0使用了分压是异常的,如果不用电阻分压那Y0也是正常的。
Y1是正常的,就Y0使用了分压是异常的,如果不用电阻分压那Y0也是正常的
您好,这里您提到只要不加分压,输出都是正常的,那排除了芯片的关系。
检查下焊接吧,或者换下电阻试试,应该是这里的问题。