Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595
HI Team
我在LMX2595的相位同步操作时,发现fOUT>15G时(即开启输出倍频器),打开SYNC功能后,PLL失锁
请问LMX2595可以进行相位同步的fOUT范围为多少?是否可以使用输出倍频器?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595
HI Team
我在LMX2595的相位同步操作时,发现fOUT>15G时(即开启输出倍频器),打开SYNC功能后,PLL失锁
请问LMX2595可以进行相位同步的fOUT范围为多少?是否可以使用输出倍频器?
谢谢
您好,您是使用TICSpro进行配置的吗?根据您的意思,输出大于15G,PLL失锁的,小于15G能正常lock是吗?
LMX2595可以进行相位同步的fOUT范围为多少?是否可以使用输出倍频器?
这个我没有找到测试数据,我会尽快给您答复。
您好,我用TICSpro试了试,可以看到红框中的提示,只有当VCO频率为20Ghz的的时候才能enable VCO doubler。

同时datasheet中也有描述,VCO倍频允许VCO频率加倍,但是只限制在20Ghz,另外,倍频同样也可以用在phase sync mode。

所以我想PLL unlock,应该不是因为phase sync mode,而是因为输出15GHz时VCO 频率没有20Ghz,不能选择VCO doubler。选择VCO输出就好。
您可以按照这个配置试试是否能lock。即选择VCO 输出到RFOUTA 15Ghz。