Part Number: CDCE62005
我按照芯片手册里的参考电路绘制了电源:

图中的4个电感我依照型号使用了1000ohm的贴片电感;电源由外部台式稳压电源提供3.3V直流电;
但出现问题:
- 此时外部电源供电电流达500mA,CDCE62005发热严重,且实际电压只有3.17V,这种压降是为什么?电流过大又是为什么?(经测量电容没有损坏)
期盼您的指点!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
关于原理图:
我看datasheet 中 30脚是接1kΩ电阻,建议您按照datasheet中的要求来:

看到有DNP字样,4脚和38脚那两个电阻您是没有焊接吗?这两个管脚是需要接10uF电容的:

40脚和41脚滤波器需要接上;
图中的4个电感我依照型号使用了1000ohm的贴片电感;
是使用的与EVM一样型号的BLM15HD102SN1D吗?
此时外部电源供电电流达500mA,CDCE62005发热严重,且实际电压只有3.17V,这种压降是为什么?电流过大又是为什么?(经测量电容没有损坏)
您是什么输出?LVDS输出,供电电流至少500mA,LVPECL输出和LVCMOS输出需要的供电电流更多,若电源提供不了这么多电流,那么供电电压降被拉低。

您测试几块板子发热严重,多测试几块板子呢以排除焊接问题
上电时,我的外部台式电源供电为3.3V,电流没有超出限制因此不会降低输出电压。
您的意思是您使用的台式3.3V电源可以提供足够的电流是吗?
电感【L13】两端电压分别为3.09V和1.7V,为什么会出现这样的压降呢?其他电感两端没有这种情况出现。
电感电流变化会在电感上产生感应电势,电感两端电压压差大说明流过电感的电流变化快或变化幅值大,您是否将VCC_VCO的滤波电容放置在CDCE管脚附近?
PCB layout 是否放置了足够多的过孔?


下面是 CDCE62005 EVM Gerber 文件,您可以参考下PCB LAYOUT: